DIO#.DIR
Description
Sets or whether the bi-directional IO is an input or output.
| Value | Description |
|---|---|
| 0 | The bi-directional IO is treated as an input signal |
| 1 | The bi-directional IO is treated as an output signal |
Examples
Context
For more information see Digital I/O.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | 0 (input) |
| Data Type | Integer |
| See Also | |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | DIO1.DIR | 0x368A | 0x1 | USINT | - | - | RW | False |
| DIO2.DIR | 0x368B | 0x1 | USINT | - | - | RW | False | |
| DIO3.DIR | 0x368C | 0x1 | USINT | - | - | RW | False | |
| DIO4.DIR | 0x368D | 0x1 | USINT | - | - | RW | False | |
| DIO5.DIR | 0x368E | 0x1 | USINT | - | - | RW | False | |
| DIO6.DIR | 0x368F | 0x1 | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|